Part Number: SN65LVCP1414
In the s4p files, which ports are the inputs and outputs?
Is there a place I can look for more information on the models?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVCP1414
In the s4p files, which ports are the inputs and outputs?
Is there a place I can look for more information on the models?
Hi Ethan,
Here is the model TI_SN65LVCP114_AMI_users_guide.pdfUser Guide
For the RX_PKG ports 1/2 are inputs and 3/4 are the outputs.
For the RX_TERM ports 1/2 are the inputs and 3/4 are the outputs
For the TX_PKG ports 1/2 are the inputs and 3/4 are the outputs
So the simulation would connect TX -> Channel -> RX_PKG -> RX_TERM -> LVCP114 IBIS -> TX_PKG -> Channel -> RX
Regards,
Lee
Thanks Lee,
I have another question.
If I'm using ADS, what component would I use for the IBIS file?
ADS can't put the IBIS file into the ReDriver_AMI or the Tx_AMI. The IBIS file can only be used for the Rx_AMI component.
Ethan
Hi Ethan,
You are correct I will look further into this model.
Regards,
Lee
Hi Ethan,
Yes, this is a relative older and limited AMI model. It only includes the Rx AMI information so it can only be used as an RX_AMI component.
Regards,
Lee