Part Number: DP83826I
Hi,
To balance heating, I am running the DP83826I ( Vdda & Vddio tied together ) on a separate 3.3V regulator from the microcontroller and other logic. The 3.3V regulators could mismatch by at most 0.14V ( e.g. +0.14V disparity, or -0.14V disparity ). The Ground as usual is identical & tied together. Also, the microcontroller seems ok with +0.3V over Vdd.
How many volts over Vdd is the DP83826I ok with for I/O signals?
Thanks,
~Alicia