Part Number: DS92LX1622
Other Parts Discussed in Thread: DS92LX1621, USB2ANY
Tool/software: TI C/C++ Compiler
Hi
I'm trying to use DS92LX1621/DS92LX1622 pair in camera mode.
i am using below circuit to connect to DS92LX1622 chip via I2C to my HOST.
at first i tied CAD pin to GND with 0ohm resistor and i used "110 0000" ID to assess the chip on HOST side the problem was that DS92LX1622 do not acknowledge the I2C packet frames.(investigated via Oscilloscope)
then i changed the RID to 2.0K and used "110 0001" ID on my I2c_master controller , now it works fine and i can easily read/write DS92LX1622 internal registers.
why it is like this?