Part Number: TPS65987D
I am developing a Type-C battery powered device that can be either a power source (Charger) or be recharged from an external charger. I want a simple 5V 3Amp advertisement for sourcing and sinking capability. I hav ethe TPS65987DDH configured with PP_HV2 as the input from my 5V power supply to supply the VBUS voltage and PP_HV1 supplying power back to my system when an external charger is applied. Does the device come programmed with a load that will support this? Is the external EEPROM shownin the EVM design required? Is there someone that can review and provide comments on the Interface design?
Thanks.