Part Number: TPS65987D
Other Parts Discussed in Thread: TPS2543, TPS65987, , TUSB422, TIDA-01620
Hello,
We have an application that's currently using a TPS2543 to enumerate a charge condition between a sinking host and a sourcing device. We're looking to add an IC between the existing circuit acting as the sourcing device that would allow use with USB-C. If the USB-C peripheral starts out as a sinking UFP and initiates a DR_SWAP command, will the TPS65987 be able to complete the sequence for the data role swap and allow the USB-C peripheral to act as a sinking DFP? Can this be done with a default configuration, and have the IC used standalone?
Regards,
Sam Dick