This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Setting for the register

Part Number: DP83822I


Hi,

Could you please let me know the register setting?

1. 0x000A - bit2 : Reading value of this bit is '0' even if default value is '1'. Is this bit has relation with boot strap setting?

2. 0x000B - bit[3:0] : Do you have recommendation setting for EtherCAT? Should it be the 1001b or 1011b?

3. 0x0017 - bit6 : Datasheet shows the default value is 0. Is it correct? I guess the default value is Normal operation (=1).

4. 0x001C - bit[10:00] : Datasheet explains "Default Value is 0x5EE" but default value is 101 1111 1111 ( =0x5FF). which value is correct?

5. 0x04D1 - bit0 :  Reading value of this bit is '1' even if EEE_EN in boot strap set to 0. Do you have reason why the bit is '1' in this condition?

Regards,
Nagata.

  • Hi Nagata,

    Are these bits that you are reading causing issues on your device? What is the core problem of the register settings you are reading? I'd like to understand what the purpose of this is based on your finding before I can explain these bits. 

    Thanks,

    Cecilia

  • Hi Cecilia,

    I will answer on behalf of Mr. Nagata.
    There is no problem in operation, but since it may be different from the value assumed here, I would like to confirm why it has changed or has changed.

    Thanks,

    Fukuda

  • Hi Fukuda,

    If there is no problem in operation and the device is working as expected I would think that you do not need to worry about the certain registers unless you know that it is directly impacting the performance. 

    If you are still wondering about the registers I will be happy to reach out to our internal team to gather these items for you. 

    Thank you,

    Cecilia

  • Hi Cecilia,

    thank you for your answer.
    However, I would like to know the details of the register, so please check with the internal team.
    Thank you,
    Fukuda
  • Hi Fukuda,

    Thank you for the feedback. I will see if I can share the details of the registers from your list.

    Thanks,

    Cecilia

  • Hello all,

    Thank you for your patience. Here are my comments below:

    0x000A Default should be 0, was this configured differently at setup?
    0x000B More info on link down modes in e2e hereL e2e.ti.com/.../565353
    0x0017 I believe this could be a typo as the normal operation should be default. Need to confirm with our internal team
    0x001C 0x05EE should be correct as it states it is 1518 bytes, again will need to confirm
    0x04D1 Can you please share the strap values you are using and what mode you have set it to?

    Thanks,

    Cecilia

  • Hi Cecilia,

    thank you for your answer.
    Let me ask you a question about each item again.

    1.0x000A-bit2: The data sheet says 1 by default. Is this a mistake?

    2.0x000B-bit[3:0]: I read the link, but I didn't understand it. Are there any problems with EtherCAT? In conclusion please tell me which is more correct, 1011 or 1001.

    3.0x0017-bit6: Please tell the confirmation result to the internal team.

    4. 0x001C-bit[10:00]: I understand that there is no problem with 0x05EE, but please check if there is a statement of 05FF in the data sheet.

    5.0x04D1-bit0: The strap value is attached, so please check it.

    Please check it.

    Thank you,


    Fukuda
  • Hi Fukuda,

    Thank you for sharing the registers, let me review your configuration and your questions above and provide feedback by EOD Wednesday.

    Thanks,

    Cecilia

  • Hi Cecilia,

    Let me explain the intent of the question about 0x04D1.
    As a result of checking the value of 0x0467, it is known that the RX_D1 pin is read in Mode1. Why is bit 0 of register 0x04D1 set to 1?
    I thought 0 was correct.
    Thanks,
    Fukuda
  • Hi Fukuda,

    This could be a datasheet typo however by default I would expect EEE_EN would be disabled. Let me confirm with our validation  team just to ensure that you are seeing the expected value.

    Just to confirm, for RX_D1 you have kept this strap open to keep it as Mode 1 correct? 

    Thanks,

    Cecilia

  • Hi Cecilia,

    RX_D1 is connected to FPGA and has a pull-down 10k ohm to make it less susceptible to noise.

    I think RX_D1 is in MODE1 because 0x0467 bit15:14 is 0, but I don't understand why 0x04D1 becomes 1.
    Thanks,
    Fukuda
  • Cecilia,

    Fukuda -san doesn't point the default value information of 0x04D1 register in datasheet.

    Let me summarize the currently status which he pointed in this forum.

    - He set  MODE 1 with RX_D1 (bootstrap). This mean is EEE_EN and PHYAD2 are disabled.
    - As he read 0x04D1 register from silicon, read value of bit-0 (EEE Capabilities Enable) is '1'.

    Q1) Are EEE_EN in bootstrap and EEE Capabilities Enable in 0x04D1 same meaning? e.g. If EEE_EN is '0', will EEE Capabilities Enable bit always be '0'?

    Q2) If Q1 is yes, Do you have reason why this mismatching among RX_D1 and 0x04D1-bit0 happened? Is there another register / bit setting to set EEE Capabilities Enable ?

    Regards,
    Nagata.

  • Hi Nagata,

    Thank you for clarifying the messages. I understand that your straps on RX_D1 are configured to Mode 1 as it is read properly on register 0x0467 meaning it should be strapped as EEE disable. However, you are seeing that for reg 0x04D1 it is contradictory saying that it is still reading as EEE capable. 

    I would expect 0x04D1 bit 0 to also read 0 as it would mean that it is disabled. I will need to review in our labs to confirm the setup and configuration.

    Can you please read back registers 0x703C and 0x703D for me? I would like to see what values are showing as the bits for the EEE advertisement.

    Thanks,

    Cecilia

  • Cecilia,

    For reading 0x703C and 0x703D registers, the procedure are

    Reading the value of register 0x703C/0x703D:

    1. reg<0x000D>=0x001F (write)

    2. reg<0x000E>=0x703C/0x703D  (write)

    3. reg<0x000D>=0x401F  (write)

    4. reg<0x000E>      (read)

    Is it correct?

    Regards,
    Nagata.

  • Hi Cecilia,

    As a result of reading with the actual device, it was confirmed that both 0x703C and 0x703D are 0 in all of bits 15-0.

    0x703C bit1 is 1 by default, but it seems to have changed to 0. [Energy Efficient Ethernet is not advertised.]
    Even if 0x04D1 bit0 is 1, if 0x703C bit1 is 0, is EEE not valid and EtherCAT has no problem?
    Thanks,
    Fukuda
  • Hi Fukuda,

    Apologies on the delay there was an error on the message reply and it looks like it did not go through on Friday.

    If 703C and 703D are confirmed as Energy Efficient Ethernet are not advertised then you are correct EEE is not valid and there could be a typo on the default reading for reg 0x4D1. 

    Thanks,

    Cecilia

  • Hi Cecilia,

    Let me confirm just in case.

    If EEE is set not to be advertised (0x703C bit1 is 0), I think that 0x04D1 bit0 is OK for both, is that correct?

    Since 0x04D1 bit0 of the own node is 1, the situation is that there is EEE capability, but is it true that the EEE of the own node is enabled when an EEE advertisement is received from the opposite node?

    Thanks,

    Fukuda

  • Hi Fukuda,

    That is a good question. I will have to confirm with our design team for this however I do not think EEE should be enabled if through register 0x703c it states that it is not being advertised. 

    Again I will have to confirm and let me provide feedback in 1 - 2 days.

    Thanks,

    Cecilia

  • Hi Fukuda,

    It seems like there is a similar question your team has asked. We have consulted this internally with our team and in order to disable EEE customer will need to program x04D1[0] = 'b0 by register write.

    https://e2e.ti.com/support/interface/f/138/t/927906?DP83822I-0x04D1-EEECFG3-register-access

    Thanks,

    Cecilia

  • Hi Cecilia,

    I have three questions.

    1. Is the Default value of 0x04D1 1 instead of 0? Is it a typo?

    2. EEE_EN is set to 0, but it is understood that it is not linked with 0x04D1 Is it correct?

    3. Some of them are mass-produced with the current register settings.
     Is there any problem with shipping as it is?

    Thanks,

    Fukuda

  • Hi Fukuda,

    The EEE_EN strap will control bit 1 of 0x703C and the default value of 0x4D1 bit 1 will be 1. Yes that is a typo. We are currently making these changes to update the datasheet accordingly.

    I am confirming with our team on the register settings and will let you know if this is ok.

    Thanks,

    Cecilia

  • Hi Fukuda

    I received some feedback from my team: 

    1. Is the Default value of 0x04D1 1 instead of 0? Is it a typo?

    Yes, default value of 0x4D1[0] is 1’b1.

    2. EEE_EN is set to 0, but it is understood that it is not linked with 0x04D1 Is it correct?

    Yes, EEE_EN strap controls only abilities in MMD7_EEE_advertisement register.

    3. Some of them are mass-produced with the current register settings.
     Is there any problem with shipping as it is?

    Even though 0x4d1[1] is set as long as 0x703c is disabled, EEE ability won't advertise although an extra next page will still be transmitted during auto negotiation. 

  • Hi Cecilia,

    The default value of bit1 of 0x703c is written as 1, but is it typo?

    Fukuda

  • Hi Cecilia,

    I'm sorry, I understand that 0x703c bit 1 is set to 0 by the strap.
    *Table 132.0x703C MMD7 Energy Efficient Ethernet Advertisement Register (MMD7_EEE_ADVERTISEMENT)

    Fukuda

  • Hi Cecilia,

    I understand about 0x04D1 but I think that 0x04D1 bit0 should change together with EEE_EN.
    I think other customers will have similar questions, so I would like you to recognize it as an issue.

    By the way, since the following questions have not been answered, please answer.
    1.0x000A-bit2: The data sheet says 1 by default. Is this a mistake?

    2.0x000B-bit[3:0]: I read the link, but I didn't understand it. Are there any problems with EtherCAT? In conclusion please tell me which is more correct, 1011 or 1001.

    3.0x0017-bit6: Please tell the confirmation result to the internal team.

    4.0x001C-bit[10:00]: I understand that there is no problem with 0x05EE, but please check if there is a statement of 05FF in the data sheet.

    Thanks

    Fukuda

  • Hi Fukuda,

    Yes as I mentioned I agreed with you that it is a typo and we will be updating in our datasheet accordingly. Thank you for letting us know that your goal was to share with future readers who may also have this confusion as well. 

    I am confirm 1-4 with our design team again as to confirm if some of these are typos or expected default values.

    Thanks for your patience I will share my answers once they provide their feedback.

    Thanks,

    Cecilia

  • Hi Fukuda,

    Feedback for questions 1-4

    1. Yes it is a typo that our team has caught which we will be revising. It should be 0 after reset

    2. No recommendations should be dependent on what mode is preferred for FLD

    3. Yes you are correct it is a typo the reset should be bit 1 normal operation

    4. Correct, this is a typo. Register 0x1C bits[10:0] has a default value of 0x5FF and not 0x5EE.

    These have already been highlighted recently and should be fixed for the next datasheet refresh.

    Thanks,

    Cecilia