Part Number: DS90UB933-Q1
Hello,
According to this below post, I know that if DS90UB933 use 8 bit mode,it could connect only the lower 8 inputs or the upper 8 inputs. Either configuration is ok. So I'd like to know if using 10bit mode, does it connect lower 10bit or upper 10bit mode? Because the datasheet described it need to use low 10bit, and DIN[10:11] are invalid, so I'd like to confirm if it could use upper 10 bit. Thank you very much.
Best regards
Kailyn