Tool/software: TI C/C++ Compiler
Our product use 954 to receive images from two 913(720p), i use the Line-Concatenate mode; but I can only see the images from RIN1
Architecture used as belows:
T T --------------RIN0-----------------913-------(720P@30fps yuv422)
| 954 |
|_ _| -----------------RIN1-----------------913------(720P@30fps yuv422)
here is my Settings
struct fpdlink_reg_struct TI954_reg_list[] = {
//{0xB3, 0x00},
{0x0c , 0x33},// enable receiver port
/*********/
{0x4C, 0x01},//rin_0 913a aliasing
//{0x72, 0xE8},//vc0 to csi-tx VC0
{0x58, 0x58},
//{0x5B, (TI913_ADDR << 1)},//??
{0x5C, (TI913_ADDR_0<<1)},
{0x5D, ISP_ADDR<<1},
{0x65, ISP_ADDR<<1},
{0x6D, 0x7c},
{0x70, 0x1E},//set RX0 RAW10_VC=0
{0x7C, 0xE0},
///********/
{0x4C, 0x12},//rin_1 913a aliasing
{0x70, 0x1E},// sensor b VC0 to csi-tx vc1
{0x58, 0x58},
//{0x5B, (TI913_ADDR << 1)},//????
{0x5C, (TI913_ADDR_1<<1)},
{0x5D, ISP_ADDR<<1},
{0x65, ISP_ADDR_1<<1},
{0x6D, 0x7c},
//{0x72, 0xE8},
{0x7C, 0x01},// FV_PO
/******/
{0x20, 0x00},// for all rx to csi0
{0x21, 0x3c},// line concatenatuon
{0x33, 0x03}, //csi en 4lan
{0x35, 0x01},
{0x1F, 0x00},// 1.6Gbps
//{0x0F, 0x7F}, //gpio out
//{0x6E, 0x10},
//{0x6F, 0x32},
};