Part Number: TCA9617B
Other Parts Discussed in Thread: TCA9517
Hi,
I have a question of how to use the I2C TCA9617B voltage translator.
I need, that the slave side should be connected to VCC from 1.8V to 5V.
Since the VCCB side provides 2.2V to 5V, my question is:
Could I connect the VCCB side to the master and VCCA side to the slave.
I have only one slave at a time, and it can work with different voltagies.
Thank you