Part Number: TCA9509
Other Parts Discussed in Thread: TCA9517, PCA9546A, PCA9306
Hi Expert,
Can we use the B port of TCA9517 to dock the B port of TCA9509, is there a problem?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Oliver,
B side of TCA9517 to B side of TCA9509 is okay. Just make sure you don't have series resistance infront of the TCA9509 B port as this may interfere with its VoL and become larger than the ViLc of the TCA9517. Assuming the logic levels are okay, I don't see a problem.
Thanks,
-Bobby
Hi Oliver,
PCA9306 does not redrive a signal, it is basically the same thing as the PCA9546A acting as a passive through element when enabled. This is why there is no input/output data in the datasheet. There will be a slight shift up from the 'input' to the 'output' due to parasitic resistance between the two sides of the device. Basically the shift up will be a function of Vshift = IoL(through device) X Ron. This shift is typically very small because Ron of PCA9306 is also very low.
Since this is all on the A side of the 9617 (thanks for choosing B version btw) I don't suspect we'll see issues in terms of input and output. 9617 has a VERY strong pull down so it should be able to pass a suitable low from A side (9617) to the 1.8V logic 'EXpander IC.' Minor shifts upwards due to 9546A pass element and 9306 pass element.
-Bobby