Part Number: TUSB320HAI
Other Parts Discussed in Thread: TUSB320, TUSB320LAI
Hello Community,
I'm using TUSB320HAI controller for my USB TypeC only requirement.
I need to configure controller as UFP in GPIO mode so I'm shorting PORT to GND directly without any Pulldown and ADDR is floating(NC) and SCL/OUT2, SDA/OUT1 also floating(NC).
CC1 CC2 are directly routed from TypeC receptacle pin and VBUS_DET is connected via 909k Resistor.
Q1 : Are above configurations correct ?
If Correct than there shouldn't be a DRP toggle on typeC receptacle pin on CC lines which is not expected. Rd should be detected everytime.Correct ?
Please let me know if I'm missing anything or is there any other dependencies for configuring controller as a UFP only Device.
Expecting an early reply .
Thanks in Advance
Regards,
Pranay.