This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI83-Q1: SN65DSI83-Q1 and Raspberry Pi CM 3+

Part Number: SN65DSI83-Q1

Hello, 

we try to use the SN65DSI83-Q1 with the Raspberry Pi CM 3+ as Chris Miller. In our case it seems that there are no problems with the MIPI interface because the PLL locks when use the MIPI clock as well as the external clock and it is possible to setup the test pattern on our LVDS Panel. Unfortunately it looks like that the frame buffer isn't send out to the MIPI interface because we can't see a change of the datastream. Furthermore we don't get any IRQs from the bridge only sometimes when we put the probe onto the interface to measure the signal. 

Is it possible to get in contact with Chris Miller to ask him which kernel version he used and how his driver looks like?

Regards 

J. Sarikas