Part Number: TPS65987D
Hello Adam,
I think that I still have problem with this evaluation kit.
Aattached is screenshot showing configuration.
If I flash the EVM from this project flash process finishes without any problem and verification is ok.
However when I reboot the EVM and read back configuration back I see that some settings are not the same. For instance my configuration for Type- C current was set to 1.5A but after reboot the configuration type- C current was set to 3.0A. To me it looks that some settings are now written correctly into flash.
The same issue happens if I create binary image using Application Customization Tool.
Also, attached is the binary image created using settings shown in screenshots from above . Please let me know If more information is required in order to resolve this issue.