Part Number: DS90UB953A-Q1
Other Parts Discussed in Thread: DS90UB954-Q1
Application :I am using DS90UB953A-Q1 to serialize mipi signals. The mipi signal is generated by xilinx FPGA mipi csi-2 tx ip core. The DS90UB954-Q1 is the deserializer used to receive serialized data from DS90UB953A-Q1 through an FPD-Link III interface. The xilinx FPGA mipi csi-2 rx ip core is used to analyze the mipi signal from DS90UB954-Q1.The lock and pass status of DS90UB954-Q1 is high.
I read the register of DS90UB953A-Q1. The value of register CSI_ERR_DLANE23 is '0x01000100'. It means 'Multi-bit Error in SYNC Sequence - Uncorrectable'. Do you know the reason of this error? There is no error in CSI_ERR_DLANE01.
Best Regards!