I am having trouble bringing up the TUSB4041I on our custom board. I've made a few mods already and the hub enumerates on the ARM side however none of the USB ports are getting 5V on VUSB. PWRON is low for all ports.
List of mods:
- USB2: Remove R127 from 1.1V regulator. Should have been a cap but can be left no popped
- USB2: Connect R113 USB2_DRVVBUS to D12 (USB_5V), cut trace to ARM
- USB2: Increase GRSTz cap to 10uF
Our VDD1.1 comes up after VDD3.3 so increased GRSTz cap to ensure reset happens after. With 10uF, reset comes up >130ms after 1.1V goes stable.