Part Number: TUSB320HAI
Other Parts Discussed in Thread: TUSB320, TUSB322I, TUSB320LAI
Hi team,
My customer considers to use TUSB320/HAI/LAI and provided some questinos.
- The data sheet shows its tDRP is 50~100ms.
Does tDRP cycle of same individual device fluctuate like "60ms cycle, then 70ms"(not device to device variation but fluctuation of device itself)? - Some of CC controller which doesn't supply VCONN doesn't connect when active cable is detected.
Does TUSB320 family can connect successfully even if active cable is connected?
Best regards,
Shota Mago