Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Hi All,
In our product, we have 2 separate USB type C ports which can be used to charge the product's battery. Let us call one of
these ports Master and one Slave. The logic of the product requires that if the Master port is already connected it will disable
the Slave port. If only the Slave port is connected, it will be able to charge the battery.
My plan was to connect each of the VBUS lines from the two connectors to the two VBUS inputs of the TPS65987, short circuit the four PP_HV lines and configure the device to sink current from both channels. I will connect all other digital lines from the two connectors (CC1,CC2, etc) through a digital mux and feed it's outputs to the TPS65987 and other units in my system. The control over the digital mux selection will be based on the VBUS line of the master so when it is present, it's digital lines will be outputted by the mux and vice versa.
I hope my explanation is clear enough and I will gladly welcome any inputs/remarks/suggestions.
Thank you,
Nir.