Part Number: DS90UB960-Q1
Hi,
I have a question regarding SLM support, when 953 is used in the sensor side:
1. For the SLM entry phase, the MIPI CSI-2 specifications suggest one option to enter SLM - that the TX (953) will enter SLM and will propagate the ULPS to the RX (960) by sending the D-PHY ULPS command on each lane (per Figure 203 in MIPI CSI-2 specifications version 3.0) - how can the user trigger entry to SLM? Does the 953 has register which holds this configuration?
2. For the SLM exit phase, the MIPI CSI-2 specifications suggest 3 options - what is the supported in the 960-953? Are all 3 options supported? How is it triggered from the 960/953 side? Does the 960/953 has registers which holds this configuration?
Thanks.
Matan