Part Number: TPS65988
Hi,
In the TP65988 EVK, I could see an internal SOURCE and external SINK path. Can I do it reverse,i.e., Can I design an internal SINK path and external SOURCE path?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65988
Hi,
In the TP65988 EVK, I could see an internal SOURCE and external SINK path. Can I do it reverse,i.e., Can I design an internal SINK path and external SOURCE path?
Hello Baghiya Lakshmi,
As per PD spec, a source path is required to have Over Current Protection (OCP). The internal power path has built in OCP That's why we recommend to use external path for sink and internal path for Source. You can use external path for Sourcing power but make sure you have external OCP.
Thanks
Prajith