Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO,
Powering the DP83TD510E-EVM using the benchtop power supply helped to get the board to connect to the USB-2-MDIO software. I believe I am using the USB-2-MDIO tool correctly and wrote the previously supplied (AutoNegotiation_Initialization and Force_1Vpp_Master_Init.txt) scripts to PHY 0 of one board and (AutoNegotiation_Initialization and Force_1Vpp_Slave_Init.txt) scripts to PHY 0 of one the other board. I made sure that in each case "Extended register access was set to "No". The boards each establish a link with the Raspberry Pis connected to their RJ45 ports but the boards do not connect to each other over the single pair I have connected between them. Can you suggest some steps I might be missing such that I can get the two boards to connect to one another via the single pair? I am going to try and include photos of the board and setup if helpful.