Part Number: DS90UA101-Q1
Other Parts Discussed in Thread: DS90UA102-Q1
Is this device protected against wrong interconnects to ethernet signaling?
We are intending to use this device to transfer audio between two products using an STP link for a commercial/consumer application.
The serializer would use an RJ45 connector as the interface between the two products to keep it user friendly.
However there is another RJ45 connector on the product for ethernet capabilities.
This is highly likely to lead to some customer wrongly inserting the ethernet link into the STP link.
Therefore, can you please advise if this would damage the part? If so, do you have any recommendations that would protect the device to allow us to use it in this scenario.
In addition, please advise where I can get information on the maturity of the device.
We need a minimum of 7yrs production lifetime and want to ensure this product will not be EOL'd.