Part Number: TUSB1044
Other Parts Discussed in Thread: TUSB1042I, HD3SS3212, TUSB1146, HD3SS3220
Hello TI and college Engineers!
First i want to thank TI for in general very nice, detailed, complete and well structured Datasheets.
However, in case of the TUSB1044 i do not understand the complete FLIP functionality.
Is there really a crosspoint switching between the Channels for SSTX/RX1 and SSTX/RX2 in that way that the cable plug orientation is corrected?
In Table 4 the there is no data-path (flippling) between RX/TX1 to RX/TX2.
Also the Schematic on Page 1, Page 19 and all the System Examples in Chapter 8.3 (Flip/No Flip) do not show a crossover mapping on the high speed data path.
Can someone clarify to me, how and what the TUSB1044 Flip functionality is working?
Our plan is to use the Redriver in a USB TypeC 3.1 gen2 x1 configuration where a corrent rx/tx lane muxing is mandatory.
Best Regards,
Dirk Jungewelter