This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS485 transreceiver with 330 ohm internal termination resistor



Dear Sir,

There is particular requirement  for the RS485 transreceiver with a SW selectable line to line termination/bias for RS485 with 330-ohm termination and 680ohm pull-up to +3.3V & 680ohm pull-down to 0 V.

Is there any part you can suggest?

BR

SM