Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869, DP83869EVM
Dear all!
I have an issue with reading from the DP83869 extended registers on the DP83869EVM.
I am using a custom NXP ls1046a processor board connected via SGMII and MDIO with the DP83869EVM. In u-boot I use the mii utility to read from the standard register set and the extended register set, reading from the extended registers with the method explained in the datasheet 9.4.9.1.7 section. I evaluate the module by reading from register OP_MODE_DECODE, GPIO_MUX_CTRL, BMCR, BMSR, PHYIDR1 and PHYIDR2. See the read transactions and the results below. The phy address is 0. I have set up the straps on the eval board to SGMII->COPPER.
BMCR, BMSR, PHYIDR1, PHYIDR2
=> mii read 0 0x0
001F
=> mii read 0 0x1
E3FF
=> mii read 0 0x2
0007
=> mii read 0 0x3
1CFF
OP_MODE_DECODE(it should be:0x40):
=> mii write 0 0x001f
=> mii write 0 0x0d 0x001f
=> mii write 0 0x0e 0x01df
=> mii write 0 0x0d 0x401f
=> mii read 0 0x0e
0001
GPIO_MUX_CTRL(it should be:0x417a):
=> mii write 0 0x0d 0x001f
=> mii write 0 0x0e 0x1e0
=> mii write 0 0x0d 0x401f
=> mii read 0 0x0e
0FFF
Am I misunderstanding the extended register read process?
Thanks,
Kristóf