This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD1983EVK: SD1983EVK's cyusb3 driver not working anymore

Part Number: SD1983EVK
Other Parts Discussed in Thread: ALP

I have an SD1983EVK and I was able to install it earlier in the year on Windows 10.

Now, after an update to Windows 10 Version 2004, the device is no longer recognized even though the driver is still installed.

I tried updating the driver, uninstalling it and installing it again using the methods discussed already in this forum.

The driver gets installed but the device is still not recognized.

On the driver event log I can see the following:

- System
- Provider
[ Name] Microsoft-Windows-Kernel-PnP
[ Guid] {9c205a39-1250-487d-abd7-e831c6290539}
EventID 400
Version 0
Level 4
Task 0
Opcode 0
Keywords 0x4000000000000000
- TimeCreated
[ SystemTime] 2020-10-23T04:02:23.0338537Z
EventRecordID 922
Correlation
- Execution
[ ProcessID] 4
[ ThreadID] 1612
Channel Microsoft-Windows-Kernel-PnP/Configuration
Computer DEV
- Security
[ UserID] S-1-5-18
- EventData
DeviceInstanceId USB\VID_0400&PID_D001\0.X.X.X.X.X.X
DriverName null
ClassGuid {00000000-0000-0000-0000-000000000000}
DriverDate
DriverVersion
DriverProvider
DriverInbox false
DriverSection
DriverRank 0x0
MatchingDeviceId
OutrankedDrivers
DeviceUpdated false
Status 0x0
ParentDeviceInstanceId USB\ROOT_HUB30\4&2a6bc02b&0&0

 

The class GUID is all zeros. 

Any assistance to solve this problem will be greatly appreciated.