Other Parts Discussed in Thread: DP83869
Dear all!
I would like to know how to correctly make a MII loopback test. My setup is a sgmii->copper the phy is connected to a NXP ls1046a processor SGMII serdes lane. From the datasheet I see that I have to configure the BMCR(0x00) reg to autoneg disable and mii loopback on and than make a software reset with the GEN_CTRL(0x1f) reg by writing 0x4000 to it. As far as I know I should ping from the interface that is connected to the phy (called fm1-mac5 in my setup) a broadcast address (10.97.0.255).
My interface config:
Ping command and the results:
The ping is not successful and the rx counter doesnt increase as well.
Am I misunderstanding loopback testing? Or is the DP83869 loopback configuration bad?
Thanks,
Kristóf