Part Number: TPS65981
4721.D1987_2_USB_PD_ONLY.pdfPS65981 with 2 x External N-FETS for a very low RDSon power path and as a power sink. See attached redacted schematic
Using 5 / 9 / 15V voltages.
We are seeing that the gate drive (X93) is only 2V above the source so the FET is not switched on and only the body diode is conducting.
X92 is 5.5V above the source and fully on.
Can you please think of any reason why the gate drive on X92 is so low pleae.
The datasheet shows that the gate drive (VGSEXT) should be between 4.5 and 7.5V
Thanks