Other Parts Discussed in Thread: DS99R421, DS90UR124
Hi,
We use DS90UR910 as deserializer to convert FPD Link to mipi CSI, and we configure it in Gen 2 mode, but nothing output now, the output signal is abnormal.
The input signal comes from car main unit, which can display on the car monitor without any problem. On the hardware level, lock pin and pass pin work fine, both of them are in high status, so what other things should we configure to make the output signal become normal, maybe some register value need to adjust? Hope to get some help. Thanks
Here is the output signal showed on the oscilloscope.