Other Parts Discussed in Thread: TCAN1051
Hello TI.
We are looking for analog switch or bus switch that can be implemented with automotive CAN bus circuit design (Protocol 11898-2:2016).
Here some requirements and conditions:
- In the new protocol the CAN absolute maximum voltage was changed to -3v to 18v (can be caused by shorten CAN signal to battery voltage) when normal operation is 0 to 5v. The required switch should not be damaged or impact the bus under those voltage levels and back to function normally when voltage levels are back to normal.
- Switch required low ON-Resistance <1 ohm and low capacitance <20pF (or the closest possible solution).
- Analog switching continuous current at Min 120mA.
- CAN Bit Rate up to 2M/Bit.
- The switch should allow bidirectional current flow.
Best Regards,
Tomer.