Part Number: TVS0701
Hi,
Our customer is designing a medical sensor patch that needs AED defib protection at the electrode inputs according to IEC60601-2-27. They're used to using MAX30034 for clamping. Can TVS0701 replace MAX30034? I'm attaching a TINA simulation of the defib discharge test for your reference. Please also check out the MAX30034 datasheet for the IEC60601-2-27 test IV curves. It's not very clear to me that TVS0701 can pass the IEC test. Please offer your feedback. Thanks.MX10_DefibTest_CM.TSC
-Kelvin