Part Number: XIO2001
[1] In the datasheet, there is an equation for calculating V_rx_cm_acp as follows.
A customer I have has pointed out that the absolute value result unit will be [V], not [V^2], so when you divide by V, you end up with no units.
This doesn't make any sense. Is the equation correct?
[2] VRX-DIFFp-p from the Datasheet lists a value of 1.2V max.
Under testing, a customer has confirmed REFCLK+ and REFCLK- are both around ±400mV, but calculating the p-p value from the equation in the datasheet, they end up with 1.6V ~ 1.7V
Is there any problem when the differential signal p-p is larger than 1.2V? Is there any chance the IC could be destroyed/malfunction?
Regards,
Darren