Part Number: TCA6424A
I plan on using this IO expander for a battery application that needs to have very low quiescent current when not operating.
VCCI will be perpetually powered by 3V3, however VCCP will be powered by a 5V auxiliary reg that can be turned off whenever the device needs to enter a low power state.
What quiescent current can I expect through VCCI while VCCP is at 0V?
Are there any other considerations I should take with the P-terminals for a low power state? I figure since everything on the P-side will be powered by the 5V auxiliary rail I shouldn't have much to worry about for leakage currents there. I also don't expect that the VCCI side should misbehave at all while VCCP is at 0v.