Part Number: TPS65988
Hi TI team,
I am using the to test the writing of the full 'flash.bin' via the 4CC commands. My initial test is the following:
- Erase the flash via the Application Customization Tool (FTDI).
- Read the flash via the Application Customization Tool (FTDI) to verify it is erased
- Use FLad to set the write start address to 0x0.
- Use FLwd to write 16 bytes of data.
- The Return Code of the FLwd is 0xFF (Error).
Could you confirm that this scenario is valid?
The script I am using has the following commands:
calling function: Raw Register Write
input value: 0x409
Input Arguments
Register Address 0x9
Write Length 4
Data 0x0
execute status: Successful write
return value: 0x0
Data
Confirmed Read 0x0
calling function: Raw Register Write
input value: 0x64614c460408
Input Arguments
Register Address 0x8
Write Length 4
Data 0x64614c46
execute status: Successful write
return value: 0x0
Data
Confirmed Read 0x0
calling function: Raw Register Read
input value: 0x109
Input Arguments
Register Address 0x9
Read Length 1
execute status: Successful read
return value: 0x0
Data
Data 0x0
calling function: Raw Register Write
input value: 0xffffffffffffffffffffffff000020001009
Input Arguments
Register Address 0x9
Write Length 16
Data 0xffffffffffffffffffffffff00002000
execute status: Successful write
return value: 0xffffffffffffffffffffffff00002000
Data
Confirmed Read 0xffffffffffffffffffffffff00002000
calling function: Raw Register Write
input value: 0x64774c460408
Input Arguments
Register Address 0x8
Write Length 4
Data 0x64774c46
execute status: Successful write
return value: 0x0
Data
Confirmed Read 0x0
calling function: Raw Register Read
input value: 0x109
Input Arguments
Register Address 0x9
Read Length 1
execute status: Successful read
return value: 0xff
Data
Data 0xff