Part Number: TPS65987D
Other Parts Discussed in Thread: TPS25750, TPS25750EVM,
I have a system which needs to charge a battery by either a PD power supply or a non PD power supply - the user may connect one kind or the other and I have no control over that.
The battery is charged using a TI charger IC.
I want to design my system so that in any case, power will be available to the charger IC and I was thinking of using this board but connect the VBUS pin DIRECTLY to the charger IC (which can handle 5 to 15 volts). I see two options here:
If a PD power supply is connected, the 65987 will negotiate a contract and the agreed power will be supplied on VBUS. If a non PD power supply is connected, the 65987 will negotiate nothing but in any case VBUS will have power (since any regular USB C power supply will power that pin)
Do you think this can work?
Nir