This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83620: Bus Contention while using with TS3L4892RHHR

Part Number: DP83620


Currently in our design we are having a two Ethernet RJ45 ports with Ethernet PHY - DP83620 along with LAN switch TS3L4892RHHR in our design.

We are planning to use this TS3L4892RHHR part as a pass through switch (connecting two RJ45 port) when the power to both Ethernet PHY power is not provided/failed and the 100Base TX signal will be looped back through the other RJ45 port by default hardware configuration of the select pin. 

During normal condition the LAN switch will be used to connect the RJ45 ports with the respective Ethernet PHY.

During the power down of the Ethernet Phy will there be any issue for the Ethernet PHY and the LAN pass through switch like bus contention or current leakage through Ethernet PHY as the switch will be powered on.

Any precaution required to be taken for the above condition considering the Eth PHY will be turned off condition and LAN switch will be powered On with the channel selected to connect both the RJ45 port.