Part Number: DP83822IF
Other Parts Discussed in Thread: AM3359
Dear Sir,
After analyzing the AM335x ICE board and AMIC ICE boards, I completed my new design using AM3359 for PRU ICSS solution(Dual Ethernet).
I have successfully booted the board but some ties Ethernet is not working properly.
Input power supply to the board: 12 V
Serial port for debug : UART0 (CP2102 chip is used to convert TTL to USB)
Scenario 1
Step 1 : Connect the 12V power supply
Step 2 : Connect the serial port (debug)
If follow the above steps then my processor will boot properly and all the peripherals are working fine.
Scenario 2
Step 1 : Connect the serial port (debug)
Step 2 : Connect the 12V power supply
If follow these steps, both the Ethernets are not working. Both the phys are detecting but the connection is not establishing. Tried to reset the boards (software reset and hardware reset) still no improvement.
Thanks in advance
Regards,
Dilrosh P S