Hello,
I'm designing a scheme for a USB-C UFP using HD3SS3220. My question is regarding the pull-up voltage of DIR pin.
It is clear that the DIR ping should pulled-up with 3.3V (see this answer), but it is also true that this voltage should be applied after VDD5 rail (see 7.3.12 VDD5 and VCC33 Power-On Requirements on ti datasheet) because it is a non-failsafe pin. I'm designing a scheme like ti suggested in the datasheet "8.2.4 Typical Application, UFP Port", and in the table 8-3 there is this statement: for VDD5 VBUS from Type-C port can be used. How is it possible? The VBUS and therefore the VDD5 can be disconnected and reconnected without any respect of VCC33 and therefore a violation of power timing for DIR pin.
Thanks in advance,
Fabio