Part Number: TIC12400
Other Parts Discussed in Thread: , SN65HVS882, SN65HVS885
Hi, I'm Luca,
we are designing a new PLC board for our sewing machines. I saw your very interesting product, the TIC12400-Q1 that I would like to use as an interface for digital / analog inputs. I have some questions to understand if I can use this component in our project:
- What are the differences between TIC12400-Q1 and TIC12400? As I understand it, the Q1 model responds to the automotive AEC-Q100 while the TIC12400 does not. The TIC12400 is recommended for PLCs, but I have read that the Vs Max (Max supply voltage) is 24Vcc with a temperature of 85 ° C, our PLC must have an operating range from 20Vcc to 28Vcc (24vDC + -15% ), if I power the TIC12400 at 28Vcc are there any problems? The TIC12400-Q1 I read that it works with a Vs Max of 35V so for our project it would be better? Strangely, the model 12400 was created for use on a PLC, but it does not support a voltage higher than 24Vdc, normally all PLCs accept at least + -10% on the 24V power supply, I don't understand ...
See also:
e2e.ti.com/.../896262
2- Another request is to monitor the status of the NPN digital inputs with an LED. In my opinion I could connect these 24 LEDs in series with PIN 1 ... 24 without resistance and adjusting the current on the PIN to 5 / 10mA. With active inputs the LEDs should light up and their voltage drop should not give me problems in the case of NPN digital inputs. In case of reading an analog signal these LEDs would disturb me, what can I do? Should I give up the LEDs?
3- If I have to read an active analog sensor, can I read its voltage? Is it sufficient to set the current to 0mA to do this?
Thanks.