This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH940-Q1: mipi output at digital reset

Part Number: DS90UH940-Q1

​Hi Team,

When 01[0] is set to 1 and the device is in digital RESET with a duration of ~2ms, the measured mipi output voltage was ~500mV.

1. Can we avoid this mipi voltage being in neither LP mode (>=550mV) nor HS mode (<=450mV)?

2. Is there anything we have to consider in such situation?

Thanks and Best Regards,
Masaru Oinaga