Part Number: SN75LVDS387
Hello TI forum,
We are currently working on a digital audio application (I2S - 1xSDATA In / 16xSDATA Out) for which it is necessary to transmit the digital audio signals over a distance of about 5m.
For this we are considering to use LVDS for the transmission from board 1 to board 2 as shown in the attached block diagram. Board 1 provides the clocks (MCLK, BCLK, FCLK) and 1x SDATA which is then transmitted via LVDS to the MCU on board 2. The MCU on board 2 is a slave to these clocks and provides 16x SDATA which is transmitted back to board 1 via LVDS. The input interface of the host on board 1 is a slave to these clocks coming from board two to account for the delay in the system.
The clocks in the system are: MCLK: 36.864MHz, BCLK: 12.288MHz, FCLK: 192kHz and we are using 3.3V signal levels
Could you please help me out with following questions:
- Do you see any issues with using a Samtec EQCD or HQCD cable (50 Ohms single ended) for the transmission? The two lines next to each other would be used for an LVDS pair (similar as mentioned in your application note SLAA284 but without the extra GND line between the LVDS pairs).
- It is planned to connect board 2 directly to a backplane. The connection cable would then go from board 1 to the backplane and then to board 2. Is this extra connector an issue in this application?
- Would the SN75LVDS series be an appropriate choice for this application or would you suggest other parts?
- Is there any benefit from using 3x 8channel LVDS devices instead of 1x16 and 1x4 channel devices as shown by the red blocks in the block diagram (skew or other issues)?
Thanks a lot,
StephanClocking scheme.pptx