Part Number: DS90UB954-Q1
Hallo,
for the forward Channel the maximum attenuation between the SerDes is 20 dB. This can i calculate If I use the typical Output Voltage (425mV eye height)) of the DS90UB953 and the minimum Input Voltage (40mV) of the DS90UB954.
Now I checked the maximum attenuation for the Back Channel. There is the typical Output Voltage of the DS90UB954 at 130 mV (eye hight) and the minimum Input Voltage of the DS90UB953 is at 120 mV. I get only 0,7 dB.
My System works good with 7,5 Meter coax cable with approx 20 dB (at 2.1 GHz) attenuation. But for the Back Channel the attenuation is by 2.5-3.5 dB (at 50 MHz).
I do not get any CRC or Parity Error with 7.5 Meter but the attenuation of the Back Channel is theoretically to high.
Where is my fault?
How can I calculate the Back Channel attenuation?