Part Number: TCAN1051GV-Q1
Other Parts Discussed in Thread: TCAN1051
Hello, I need another set eye, confirming that TCAN1051GV-Q1 is substituted/ drop-in replacement for TJA1051TK/3/1J.
currently, I don't see an issue, is this the case
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1051GV-Q1
Other Parts Discussed in Thread: TCAN1051
Hello, I need another set eye, confirming that TCAN1051GV-Q1 is substituted/ drop-in replacement for TJA1051TK/3/1J.
currently, I don't see an issue, is this the case
thanks
Hi Allen,
Yes, TCAN1051GV-Q1 is pin-to-pin compatible with TJA1051 and supports the same functionality. The main differences in specifications based on the datasheets are ESD ratings (varies), rated bus differential (TCAN: +-58V, TJA +-27V), and loop timing (TCAN: 175ns, TJA: 220ns). No special considerations are needed when swapping to TCAN1051 in most systems.
Regards,
Eric Schott