This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH928Q-Q1: Acceptable insertion loss , return loss

Part Number: DS90UH928Q-Q1
Other Parts Discussed in Thread: DS90UB953-Q1,

Hi team

I need to know about acceptable insertion loss and return loss.

I found the thread about DS90UB953-Q1.

maximum allowed Insertion loss for the DS90UB953-Q1 can be applied to DS90UH928Q-Q1?

I also need maximum allowed return loss.

Thanks

Maximum allowed Insertion loss for the transmission channel are:

Frequency Insertion loss (dB)

1MHz -1.4

5MHz -2.3

10MHz -2.5

50MHz -3.5

100MHz -4.5

500MHz -9.5

1GHz -14