Part Number: TPS25750
In a previous thread it was stated:
"When there is no power on VIN_3V3 and the TPS25750 is powered from VBUS, the current is being supplied by the charger at the other end of the Type-C cable which by the Type-C spec must be able to provide a minimum of 900mA.
Also, this state should only be temporary."
Can this be confirmed that it should only be temporary? Why is this the case?
In a sink-only application, VBUS will always be available to power the TPS25750 and all internal circuitry will be powered through VBUS.