This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-Q1: Without Back-Channel no serial stream output?

Part Number: DS90UB913A-Q1

Hello,

Is DS90UB913A inactive when the back-channel of Des is configured OFF (DS90UB914A "BC Enable", 0x01 bit 2 is 0)?

If so, what state is Ser in when Des is configured as above? Only the differential driver is OFF?

Is this the case also for the combination of UB913A and UB936, and others?

Thank you.

Regards,

Oguri (TIJ automotive FAE)