Part Number: USB-C-PD-DUO-EVM
Other Parts Discussed in Thread: TPS65981
Followed the procedure as described in USB-C-PD-DUO-EVM User's Guide.
Tried even to restore with the recovery bin files for source and sink under C:\Program Files\Texas Instruments\TPS65981_2_6_7_8 Application Customization 6.1.1\tps6598x-application-customization\recovery.
Reading the flash gives as result for the sink / source binaries (Jumper J202 in SNK / SRC position) all zero files.
Those files are also very large, compared with the source and sink binary file sizes (1024kB).
Measured also on TP3 only 2.3V and 3.3V is required. But the sink 3.3V is OK. So do not understand why both source and sink cannot be flashed.
I2C address sweep on sink only (powered from USB-C) gives 0x21. I2C address sweep on source (jumper J202 in SRC position) gives an address list from 0x00 to 0xFE. See attachements.
What's wrong with the USB-C-PD-DUO-EVM?
Is there something in the set-up that is not correct or is the I2C address list on the source device related to the 2.3V instead of the 3.3V?
But why thus the sink device not flash as only one I2C address listed?