Part Number: DP83TC811EVM
I'm having a hard time figuring out how to interface with the Automotive Ethernet header (J7) on the DP83TC811EVM. I need a cable that will plug into the dev board on one end and have pigtails on the other. Here's what I've found so far:
Header (J7): TE 9-2304372-9 MATEnet Header
Frame: TE 9-2302454-9 MATEnet Frame
But the Frame is basically and empty shell, there's no pins that actually plug into the header. So then it seems like I need an additional housing that goes inside the frame?
Housing: TE 2302450-1 Housing for Female Terminals
But the Housing doesn't have the pins either so then it seems like I also need the corresponding sockets (assuming the header is male?):
Pins: TE 1-1703930-2 Nano MQS Receptacle Terminals
I would like to avoid buying all the subcomponents myself and assembling the cable so I'm hoping to find a premade cable assembly. The User Guide calls out a B-type automotive connector:

This led me to the TE Cable Spec

Is the type cable shown there what I need? Where is the best place to buy one?