This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: What is the maximum resolution of DP output with signal MIPI DSI input port?

Part Number: SN65DSI86


Hi David,

I do some calculate, it seem SN65DSI86 can support 3840 x 2160 30fps, 24bpp via 4-lane MIPI DSI.

Following is my calculation, please help to check about this:

Steam bit rate = 3840 x 2160 x 30 x 24 ≈ 6Gbps

Min_number of DSI lanes = 6Gbp / 2 x 750MHz = 6G / 1.5G = 4