This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: DP83867ISRGZR

Part Number: DP83867IS

Hi,

We have used TI PHY (DP83867ISRGZR) and other protection circuits in our board to power-up using PoE of 48V through RJ-45 connector.

It is designed to have an option for power-up using both DC supply and PoE with PHY DP83867ISRGZR.

When we were using dc supply to power the board and using normal ethernet, the board was working properly with 1Gbps link speed.

After we started powering-up with PoE, observed failures over time.

Detail testing exercise done is as below:

  1. 48V dc power is given at pair C and pair D using PoE adaptor.
  2. Initially it was working properly with successful auto-negotiation completion and link establishment.
  3. When multiple (10 times) plug-in and plug-out of RJ-45 was performed, auto-negotiation has not been able to complete successfully and link didn’t establish.
  4. Then it is observed that there is variation in impedance (measured w.r.t. TPAD pin) at PHY Differential Transmit and Receive Signal Pins (Pin No. 7 and 8, 10 and 11). They are getting low.
  5. We have observed this issue on 4-5 chipsets.

So, Kindly check and provide us the solution.

Please find the detail circuit design that we have used at below link.

/cfs-file/__key/communityserver-discussions-components-files/138/PoE-Problem-Statement.docx

Thanks

Jyoti Agrawal