HI I,K:
We have screen parameters and use DSI tuner to configure sn65dsi84. But now we have some problems, which are very urgent.
1、we use Flatlink Output Data (Format 2); Single-Link 24 Bpp,Here are our screen parameters.
2、The following is our configuration using DSI tuner. In order to make the LVDS line time match the DSI line time, I added DSI_ HPW to 1340. However, after the initialization sequence is completed, register 0xe5 is equal to 0x01. Can you tell me if there is a problem with the configuration, and if so, what is the reason?